Raritan EMX JSON-RPC API
|
Classes | |
interface | AlarmManager |
AlarmManager interface. More... | |
interface | Channel_1_0_1 |
Event Channel. More... | |
interface | DataPushService_1_0_1 |
Data push service configuration interface. More... | |
interface | Engine_1_0_1 |
There is a single event engine instance reachable by a well known reference. More... | |
struct | Event |
Event has a type: a STATE event indicates that a boolean state has been changed, i.e. More... | |
struct | KeyValue |
Helper that is used wherever key/value pairs are required. More... | |
interface | Service_1_0_1 |
Event Service. More... | |
interface | TimerEventManager_2_0_0 |
TimerEventManager interface. More... | |
Variables | |
valueobject | UserEvent |
This UserEvent may be used as base valueobject for all concrete events that are triggered because of user interaction. More... | |
string | actIpAddr |
ip or device on which user is logged in | |
Event interface.
valueobject event::UserEvent |
This UserEvent may be used as base valueobject for all concrete events that are triggered because of user interaction.
user who triggered event