Raritan EMX JSON-RPC API
|
Network Configuration. More...
Classes | |
struct | CommonInfo |
Common info. More... | |
struct | CommonSettings_2_0_0 |
Common settings. More... | |
interface | Diagnostics |
Diagnostics interface. More... | |
struct | DnsInfo |
DNS info. More... | |
struct | DnsSettings_2_0_0 |
DNS settings. More... | |
struct | EapAuthSettings_3_0_0 |
EAP authentication settings. More... | |
struct | EthInfo_1_0_1 |
Ethernet interface info. More... | |
struct | EthLinkMode |
Ethernet link mode. More... | |
struct | EthSettings_2_0_0 |
Ethernet interface settings. More... | |
struct | Info_1_0_1 |
Network info. More... | |
struct | InterfaceInfo |
Interface specific info. More... | |
struct | InterfaceIpSettings_2_0_0 |
Interface specific IP settings. More... | |
struct | InterfaceIPv4Info |
Interface specific IPv4 info. More... | |
struct | InterfaceIPv6Info |
Interface specific IPv6 info. More... | |
struct | InterfaceSettings_2_0_0 |
Interface specific settings. More... | |
struct | IpAddrCidr |
IPv4/IPv6 address and prefix len. More... | |
struct | IpRoute |
IPv4/IPv6 route. More... | |
struct | IpRoutingSettings_2_0_0 |
IP protocol specific routing settings. More... | |
interface | Net_5_0_0 |
Network configuration interface. More... | |
struct | PortForwardingInfo |
Port forwarding info. More... | |
struct | PortForwardingMasterAddrInfo |
Port forwarding master address info for an interface. More... | |
struct | PortForwardingProtocolMapping |
Mapping from application protocol id to name and transport protocol. More... | |
struct | PortForwardingSettings_2_0_0 |
Port forwarding settings. More... | |
struct | RoutingInfo |
Routing info. More... | |
struct | RoutingSettings_2_0_0 |
Routing settings. More... | |
interface | Services |
Network services configuration interface. More... | |
struct | ServiceSettings |
Network service settings. More... | |
struct | Settings_3_0_0 |
Network settings. More... | |
struct | WlanInfo |
WLAN interface info. More... | |
struct | WlanSettings_3_0_0 |
WLAN interface settings. More... | |
Enumerations | |
enum | PortForwardingRole { MASTER, SLAVE } |
Role of the node when port forwarding is enabled. More... | |
enum | IpConfigMethod { STATIC, DHCP, AUTO } |
IP configuration method. More... | |
enum | InterfaceType { ETHERNET, WLAN, BRIDGE } |
The interface type. More... | |
enum | InterfaceOpState { NOT_PRESENT, DOWN, NO_LINK, UP } |
Interface operational state. More... | |
enum | EapOuterAuthMethod_2_0_0 { EAP_PEAP, EAP_TLS } |
EAP outer authentication method. More... | |
enum | EapInnerAuthMethod_2_0_0 { INNER_EAP_MSCHAPv2, INNER_EAP_TLS } |
EAP inner authentication method. More... | |
enum | EapStatus { EAP_STATUS_DISABLED, EAP_STATUS_PENDING, EAP_STATUS_FAILED, EAP_STATUS_SUCCESS } |
EAP authentication status. More... | |
enum | EthSpeed { SPEED_AUTO, SPEED_MBIT_10, SPEED_MBIT_100, SPEED_MBIT_1000 } |
Ethernet speed. More... | |
enum | EthDuplexMode { DUPLEX_MODE_AUTO, DUPLEX_MODE_HALF, DUPLEX_MODE_FULL } |
Ethernet duplex mode. More... | |
enum | EthAuthType { ETH_AUTH_NONE, ETH_AUTH_EAP } |
Ethernet authentication type. More... | |
enum | WlanSecProtocol { WPA2 } |
WLAN security protocol. More... | |
enum | WlanAuthType_2_0_0 { WLAN_AUTH_NONE, WLAN_AUTH_PSK, WLAN_AUTH_EAP } |
WLAN authentication type. More... | |
enum | WlanChannelWidth { CHANNEL_WIDTH_UNKNOWN, CHANNEL_WIDTH_20_NO_HT, CHANNEL_WIDTH_20, CHANNEL_WIDTH_40, CHANNEL_WIDTH_80, CHANNEL_WIDTH_80P80, CHANNEL_WIDTH_160 } |
WLAN channel width. | |
Variables | |
valueobject | CommonInfoChangedEvent |
Event that is send when common network info has changed. More... | |
valueobject | InterfaceInfoChangedEvent |
Event that is send when common interface specific network info has changed. More... | |
valueobject | EthInfoChangedEvent_1_0_1 |
Event that is send when ethernet interface specific network info has changed. More... | |
string | ifLabel |
interface label | |
EthInfo_1_0_1 | ethInfo |
Current ethernet interface specific info. | |
valueobject | WlanInfoChangedEvent |
Event that is send when WLAN interface specific network info has changed. More... | |
WlanInfo | wlanInfo |
Current WLAN interface specific info. | |
valueobject | LinkStateChangedEvent |
Event that is send when the operational state of an interface changed. More... | |
InterfaceType | ifType |
interface type | |
InterfaceOpState | ifState |
Current operational interface state. | |
valueobject | PortForwardingSlavePresenceStateChangedEvent |
Event that is send when the presence state of a downstream port forwarding slave changes. More... | |
Network Configuration.
Network services configuration.
enum net::EapStatus |
enum net::EthAuthType |
enum net::EthDuplexMode |
enum net::EthSpeed |
enum net::InterfaceType |
enum net::IpConfigMethod |
enum net::WlanSecProtocol |
valueobject net::CommonInfoChangedEvent |
Event that is send when common network info has changed.
Current common network info
valueobject net::EthInfoChangedEvent_1_0_1 |
Event that is send when ethernet interface specific network info has changed.
Ethernet interface name
valueobject net::InterfaceInfoChangedEvent |
Event that is send when common interface specific network info has changed.
Current common interface specific info
valueobject net::LinkStateChangedEvent |
Event that is send when the operational state of an interface changed.
interface name
valueobject net::PortForwardingSlavePresenceStateChangedEvent |
Event that is send when the presence state of a downstream port forwarding slave changes.
true
when a slave is present
valueobject net::WlanInfoChangedEvent |
Event that is send when WLAN interface specific network info has changed.
WLAN interface name