Raritan PX2/PX3 JSON-RPC API
Server Reachability Monitoring

The server reachability monitor is configured via the servermon.ServerMonitor interface at the well-known URI /servermon. Monitored servers are managed with the addServer, modifyServer and deleteServer methods and retrieved with listServers and getServers.

# Python example: Monitor a new server
import raritan.rpc.servermon
server = raritan.rpc.servermon.ServerMonitor.ServerSettings(
host = "8.8.8.8",
enabled = True,
pingInterval = 60, # seconds
retryInterval = 5, # seconds
activationCount = 15,
failureCount = 5,
resumeDelay = 180, # seconds
resumeCount = 5
)
server_monitor = raritan.rpc.servermon.ServerMonitor("/servermon", agent)
server_monitor.addServer(server)

Reacting to Server Status Changes

Server status changes raise events that can be used to trigger event rules. See Event Rules and Actions for details. The second component in the event ID is the server's host name in the exact notation of the server settings. For example, an event rule for the server in the example above would select event IDs like [ "Server", "8.8.8.8", "Unreachable" ]. It is possible to use the wildcard * as host name to select events for all monitored servers.

The following events are emitted for monitored servers.