Raritan PX2/PX3 JSON-RPC API
|
User Management More...
Classes | |
struct | Account |
Account information More... | |
struct | AuxInfo |
Auxiliary user information. More... | |
struct | Preferences |
User preferences More... | |
interface | Role |
Role management interface More... | |
interface | RoleManager |
Role manager interface. More... | |
struct | SnmpV3Settings |
SNMPv3 settings. More... | |
interface | User_1_0_2 |
User interface More... | |
struct | UserCapabilities |
User Capabilities Describe if certain operations can be performed for user. More... | |
struct | UserInfo |
User information More... | |
interface | UserManager_1_0_3 |
User manager interface More... | |
Enumerations | |
enum | TemperatureEnum { DEG_C, DEG_F } |
Preferred display unit for temperature sensors. More... | |
enum | LengthEnum { METER, FEET } |
Preferred display unit for length measurements, e.g. More... | |
enum | PressureEnum { PASCAL, PSI } |
Preferred display unit for (air) pressure sensors. More... | |
Variables | |
valueobject | RoleEvent |
Base type of all account event. | |
valueobject | RoleAdded |
valueobject | RoleRemoved |
valueobject | RoleChanged |
Role::Info | newSettings |
valueobject | AccountEvent |
Base type of all account event. More... | |
valueobject | AccountAdded |
This event is emitted after a new account with the provided username was added. | |
valueobject | AccountRemoved |
This event is emitted after the account with the provided username has been removed. | |
valueobject | PasswordChanged |
This event is emitted after the password for an account was changed. | |
valueobject | AccountChanged |
This event is emitted if the settings of an account as defined in usermgmt::UserInfo have changed (Note: we may add an indication what in the structure has changed or even split the event, if handling is difficult) | |
User Management
enum usermgmt::LengthEnum |
valueobject usermgmt::AccountEvent |
Base type of all account event.
id of user which was affected