Raritan PX2/PX3 JSON-RPC API
|
Peripheral Devices. More...
Classes | |
struct | Address_3_0_1 |
peripheral device position based address More... | |
struct | DeviceID_3_0_1 |
peripheral device identification More... | |
interface | DeviceManager_3_0_0 |
Peripheral Device Manager. More... | |
interface | DeviceSlot_2_0_2 |
Peripheral Device Slot. More... | |
interface | DoorHandleControllerPackage |
interface | G2Production_4_0_0 |
interface | Package |
struct | PackageInfo_2_0_0 |
Peripheral device package information. More... | |
struct | PosElement |
peripheral device position element, list forms position More... | |
Enumerations | |
enum | PortType { ONEWIRE_ONBOARD, ONEWIRE_DEV_PORT, ONEWIRE_HUB_PORT, ONEWIRE_CHAIN_POS } |
peripheral device port types More... | |
Variables | |
valueobject | Device_3_0_1 |
A peripheral device is the collection of. More... | |
vector< PosElement > | position |
Position within 1-wire topo. | |
string | packageClass |
physical package identifier | |
sensors::Sensor_4_0_2 | device |
device reference | |
Peripheral Devices.
enum peripheral::PortType |
valueobject peripheral::Device_3_0_1 |
A peripheral device is the collection of.