Raritan EMX JSON-RPC API
Classes | Enumerations | Variables
net Module Reference

Network Configuration. More...

Classes

struct  CommonInfo
 Common info. More...
 
struct  CommonSettings_2_0_0
 Common settings. More...
 
interface  Diagnostics
 Diagnostics interface. More...
 
struct  DnsInfo
 DNS info. More...
 
struct  DnsSettings_2_0_0
 DNS settings. More...
 
struct  EapAuthSettings_3_0_0
 EAP authentication settings. More...
 
struct  EthInfo_1_0_1
 Ethernet interface info. More...
 
struct  EthLinkMode
 Ethernet link mode. More...
 
struct  EthSettings_2_0_0
 Ethernet interface settings. More...
 
struct  Info_1_0_1
 Network info. More...
 
struct  InterfaceInfo
 Interface specific info. More...
 
struct  InterfaceIpSettings_2_0_0
 Interface specific IP settings. More...
 
struct  InterfaceIPv4Info
 Interface specific IPv4 info. More...
 
struct  InterfaceIPv6Info
 Interface specific IPv6 info. More...
 
struct  InterfaceSettings_2_0_0
 Interface specific settings. More...
 
struct  IpAddrCidr
 IPv4/IPv6 address and prefix len. More...
 
struct  IpRoute
 IPv4/IPv6 route. More...
 
struct  IpRoutingSettings_2_0_0
 IP protocol specific routing settings. More...
 
interface  Net_5_0_0
 Network configuration interface. More...
 
struct  PortForwardingInfo
 Port forwarding info. More...
 
struct  PortForwardingMasterAddrInfo
 Port forwarding master address info for an interface. More...
 
struct  PortForwardingProtocolMapping
 Mapping from application protocol id to name and transport protocol. More...
 
struct  PortForwardingSettings_2_0_0
 Port forwarding settings. More...
 
struct  RoutingInfo
 Routing info. More...
 
struct  RoutingSettings_2_0_0
 Routing settings. More...
 
interface  Services
 Network services configuration interface. More...
 
struct  ServiceSettings
 Network service settings. More...
 
struct  Settings_3_0_0
 Network settings. More...
 
struct  WlanInfo
 WLAN interface info. More...
 
struct  WlanSettings_3_0_0
 WLAN interface settings. More...
 

Enumerations

enum  PortForwardingRole { MASTER, SLAVE }
 Role of the node when port forwarding is enabled. More...
 
enum  IpConfigMethod { STATIC, DHCP, AUTO }
 IP configuration method. More...
 
enum  InterfaceType { ETHERNET, WLAN, BRIDGE }
 The interface type. More...
 
enum  InterfaceOpState { NOT_PRESENT, DOWN, NO_LINK, UP }
 Interface operational state. More...
 
enum  EapOuterAuthMethod_2_0_0 { EAP_PEAP, EAP_TLS }
 EAP outer authentication method. More...
 
enum  EapInnerAuthMethod_2_0_0 { INNER_EAP_MSCHAPv2, INNER_EAP_TLS }
 EAP inner authentication method. More...
 
enum  EapStatus { EAP_STATUS_DISABLED, EAP_STATUS_PENDING, EAP_STATUS_FAILED, EAP_STATUS_SUCCESS }
 EAP authentication status. More...
 
enum  EthSpeed { SPEED_AUTO, SPEED_MBIT_10, SPEED_MBIT_100, SPEED_MBIT_1000 }
 Ethernet speed. More...
 
enum  EthDuplexMode { DUPLEX_MODE_AUTO, DUPLEX_MODE_HALF, DUPLEX_MODE_FULL }
 Ethernet duplex mode. More...
 
enum  EthAuthType { ETH_AUTH_NONE, ETH_AUTH_EAP }
 Ethernet authentication type. More...
 
enum  WlanSecProtocol { WPA2 }
 WLAN security protocol. More...
 
enum  WlanAuthType_2_0_0 { WLAN_AUTH_NONE, WLAN_AUTH_PSK, WLAN_AUTH_EAP }
 WLAN authentication type. More...
 
enum  WlanChannelWidth {
  CHANNEL_WIDTH_UNKNOWN, CHANNEL_WIDTH_20_NO_HT, CHANNEL_WIDTH_20, CHANNEL_WIDTH_40,
  CHANNEL_WIDTH_80, CHANNEL_WIDTH_80P80, CHANNEL_WIDTH_160
}
 WLAN channel width.
 

Variables

valueobject CommonInfoChangedEvent
 Event that is send when common network info has changed. More...
 
valueobject InterfaceInfoChangedEvent
 Event that is send when common interface specific network info has changed. More...
 
valueobject EthInfoChangedEvent_1_0_1
 Event that is send when ethernet interface specific network info has changed. More...
 
string ifLabel
 interface label
 
EthInfo_1_0_1 ethInfo
 Current ethernet interface specific info.
 
valueobject WlanInfoChangedEvent
 Event that is send when WLAN interface specific network info has changed. More...
 
WlanInfo wlanInfo
 Current WLAN interface specific info.
 
valueobject LinkStateChangedEvent
 Event that is send when the operational state of an interface changed. More...
 
InterfaceType ifType
 interface type
 
InterfaceOpState ifState
 Current operational interface state.
 
valueobject PortForwardingSlavePresenceStateChangedEvent
 Event that is send when the presence state of a downstream port forwarding slave changes. More...
 

Detailed Description

Network Configuration.

Network services configuration.

Enumeration Type Documentation

◆ EapInnerAuthMethod_2_0_0

EAP inner authentication method.

Enumerator
INNER_EAP_MSCHAPv2 

MSCHAPv2 authentication.

INNER_EAP_TLS 

TLS authentication.

◆ EapOuterAuthMethod_2_0_0

EAP outer authentication method.

Enumerator
EAP_PEAP 

PEAP authentication.

EAP_TLS 

TLS authentication.

◆ EapStatus

EAP authentication status.

Enumerator
EAP_STATUS_DISABLED 

EAP authentication disabled.

EAP_STATUS_PENDING 

EAP authentication pending.

EAP_STATUS_FAILED 

EAP authentication failed.

EAP_STATUS_SUCCESS 

EAP authentication succeeded.

◆ EthAuthType

Ethernet authentication type.

Enumerator
ETH_AUTH_NONE 

No authentication.

ETH_AUTH_EAP 

802::1x (EAP) authentication

◆ EthDuplexMode

Ethernet duplex mode.

Enumerator
DUPLEX_MODE_AUTO 

Use auto-negotiation to set duplex mode.

DUPLEX_MODE_HALF 

Half duplex.

DUPLEX_MODE_FULL 

Full duplex.

◆ EthSpeed

Ethernet speed.

Enumerator
SPEED_AUTO 

Use auto-negotiation to set speed.

SPEED_MBIT_10 

10 MBit/s

SPEED_MBIT_100 

100 MBit/s

SPEED_MBIT_1000 

1000 MBit/s (1 GBit/s)

◆ InterfaceOpState

Interface operational state.

Enumerator
NOT_PRESENT 

Interface is not present.

DOWN 

Interface is down.

NO_LINK 

Interface has no link.

UP 

Interface is up and running.

◆ InterfaceType

The interface type.

Enumerator
ETHERNET 

Ethernet interface.

WLAN 

WLAN interface.

BRIDGE 

Bride interface.

◆ IpConfigMethod

IP configuration method.

Enumerator
STATIC 

No automatic configuration.

DHCP 

Use DHCP for automatic configuration (IPv4 only)

AUTO 

Use automatic configuration (IPv6 only)

◆ PortForwardingRole

Role of the node when port forwarding is enabled.

Enumerator
MASTER 

Node is the port forwarding master.

SLAVE 

Node is a port forwarding slave.

◆ WlanAuthType_2_0_0

WLAN authentication type.

Enumerator
WLAN_AUTH_NONE 

No authentication.

WLAN_AUTH_PSK 

Pre-shared key authentication.

WLAN_AUTH_EAP 

802::1x (EAP) authentication

◆ WlanSecProtocol

WLAN security protocol.

Enumerator
WPA2 

WPA2 security protocol.

Variable Documentation

◆ CommonInfoChangedEvent

valueobject net::CommonInfoChangedEvent

Event that is send when common network info has changed.

Current common network info

◆ EthInfoChangedEvent_1_0_1

valueobject net::EthInfoChangedEvent_1_0_1

Event that is send when ethernet interface specific network info has changed.

Ethernet interface name

◆ InterfaceInfoChangedEvent

valueobject net::InterfaceInfoChangedEvent

Event that is send when common interface specific network info has changed.

Current common interface specific info

◆ LinkStateChangedEvent

valueobject net::LinkStateChangedEvent

Event that is send when the operational state of an interface changed.

interface name

◆ PortForwardingSlavePresenceStateChangedEvent

valueobject net::PortForwardingSlavePresenceStateChangedEvent

Event that is send when the presence state of a downstream port forwarding slave changes.

true when a slave is present

◆ WlanInfoChangedEvent

valueobject net::WlanInfoChangedEvent

Event that is send when WLAN interface specific network info has changed.

WLAN interface name